0611CT1603

Connection terminals

Flat copper surface, linked to the conducting parts of the circuit breaker and to which power connections are made using bars, connectors or lugs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.