0611CT1603

Durability

The term "durability" is used in the standards instead of "endurance" to express the expectancy of the number of operating cycles which can be performed by the equipment before repair or replacement of parts. The term "endurance" is used for specifically defined operational performance.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.