0611CT1603

Neutral protection (IN)

The neutral is protected because all circuit breaker poles are interrupted. The PowerPacT B-frame 4P circuit breaker has fixed 100% protection in the far left pole.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.