0611CT1603

Direct rotary handle

This is an optional control handle for the circuit breaker. It has the same three positions I (ON), O (OFF) and TRIPPED as the toggle control. It provides IP40, IK07 and the possibility, due to its extended travel, of using early-make and earlybreak contacts. It maintains suitability for isolation and offers optional locking using a padlock.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.