0611CT1603

Current-limiting circuit breaker IEC 60947-2

"A Circuit breaker with a break-time short enough to prevent the short-circuit current reaching its otherwise attainable peak value".
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.