0611CT1603

Rated short-time withstand current (Icw)

"Value of short-time withstand current, assigned to the equipment by the manufacturer, that the equipment can carry without damage, under the test conditions specified in the relevant product standard". Generally expressed in kA for 0.5, 1 or 3 seconds. This is an essential characteristic for air circuit breakers. It is not significant for molded-case circuit breakers for which the design targets fast opening and high limiting capacity.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.