0611CT1603

Circuit breaker IEC 60947-2

"Mechanical switching device, capable of making, carrying and breaking currents under normal circuit conditions and also making, carrying for a specified time and breaking currents under specified abnormal circuit conditions such as those of short circuit". Circuit breakers are the device of choice for protection against overloads and short-circuits. Circuit breakers may, as is the case for PowerPacT, be suitable for isolation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.