0611CT1603

Let-Through Curves and Trip Curves

PowerPacT B-Frame Let-Through Energy Curve

PowerPacT B-Frame Peak Let-Through Current Curve

PowerPacT B-Frame 15/20 A Thermal-Magnetic Trip

Refer to Trip Units for magnetic trip levels on 250 Vdc systems.

PowerPacT B-Frame 25/30 A Thermal-Magnetic Trip

Refer to Trip Units for magnetic trip levels on 250 Vdc systems.

PowerPacT B-Frame 35/50 A Thermal-Magnetic Trip

Refer to Trip Units for magnetic trip levels on 250 Vdc systems.

PowerPacT B-Frame 60/100 A Thermal-Magnetic Trip

Refer to Trip Units for magnetic trip levels on 250 Vdc systems.

PowerPacT B-Frame 110/125 A Thermal-Magnetic Trip

Refer to Trip Units for magnetic trip levels on 250 Vdc systems.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.