0611CT1603

Non-tripping time

This is the minimum time during which the protective device does not operate in spite of pick-up overrun, if the duration of the overrun does not exceed the corresponding voluntary time delay.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.