0611CT1603

Relay (electrical) IEC 60947-1

"Device designed to produce sudden, predetermined changes in one or more electrical output circuits when certain conditions are fulfilled in the electrical input circuits controlling the device".
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.