0611CT1603

Contactor IEC 60947-1

"Mechanical switching device having only one position of rest, operated otherwise than by hand, capable of making, carrying and breaking currents under normal circuit conditions including operating overload conditions". A contactor is provided for frequent opening and closing of circuits under load or slight overload conditions. It must be combined and coordinated with a protective device against overloads and short-circuits, such as a circuit breaker.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.