0611CT1603

Vibration withstand IEC 60068-2-6

Circuit breakers are tested in compliance with standard IEC 60068-2-6 for the levels required by merchant-marine inspection organisations (Veritas, Lloyd's, etc.):
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.