BQT2430700_03

Control from C-Bus

In order to be used, a dimmer channel must be assigned a group address from one of the four available Lighting Application addresses that can be configured in the dimmer unit. The same group address can be assigned to multiple channels.

NOTE: Unused channels should be left without a group address configured.

More advanced settings can be configured to modify the conditions required for the dimmer channel to turn on. The advanced settings are:

  • Logic

  • Power-On Delay

  • Warn Before Off

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?