BQT2430700_03

Remote Override

The extra two pairs of the C-Bus Network cable provide high priority override functions for most C-Bus Output units.

  • The Green & Green/White pair is used for the Remote ON function.

  • The Brown & Brown/White pair is used for the Remote OFF function.

Connecting either pair to the C-Bus negative pair activates the corresponding function.

Each dimmer channel can be individually included or excluded from either or both of the Remote ON and Remote OFF functions. By default, all channels are included in both. This setting can be changed using the SpaceLogic C-Bus Commission software.

The SpaceLogic C-Bus Network Automation and Application Controllers provide facilities to control these overrides.

IMPORTANT: During the installation, it is important to make sure these pairs are not left unterminated, as this may cause the override functions to be triggered by accident.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?