Measurement Application
The Measurement Application is used for broadcasting values of physical parameters monitored by C-Bus devices.
The measured quantities can be displayed on devices with graphical user interfaces such eDLTs or Automation Controllers, and can be used as inputs to automation in SpaceLogic C-Bus Automation Controllers.
Measurement Application message contains the following information:
-
A device ID to identify the unit which broadcast the message.
-
The channel number, which is used to differentiate between multiple measurements that the single device may produce.
-
The measured value.
-
The units of the measured value (example: Volts, Amperes, Degrees).
The C-Bus Digital Dimmers provide measurements of the following values via the Measurement Application which can be useful for monitoring the health of the unit, or for detecting abnormal conditions:
|
Channel Number |
Quantity |
Units |
|
0-7 |
Channel 1 — Channel 8 Lamp Running Time |
Hours |
|
128-135 |
Channel 1 — Channel 8 Operating Temperature |
°C |
|
252 |
Power Supply Load Current |
Amperes |
|
253 |
C-Bus Voltage |
Volts |
|
254 |
Unit Operating Temperature |
°C |
Measurements can be configured to broadcast periodically, by setting the measurement periodic broadcast parameter. This can be set to an interval between 1 and 254 minutes.
In addition, individual quantities may be excluded from the regular broadcast by de-selecting them in the Measurement Regular Broadcast options parameter.
The Lamp Running Time measurements can be reset to zero by configuring a Trigger Group and sending a trigger event on that Trigger Group with the action selector set to the channel which is to be cleared, or an Action Selector of 255 to clear all channels simultaneously.