BQT2430700_03

Power on Delay

Each channel has a configurable power-on delay parameter, which can be used to delay the recovery of the channel state upon restoration of power after a power loss. This can be used to help manage inrush for the installation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?