BQT2430700_03

Power-Up Load Status

While designing an installation, it is important to understand the power-up behaviour of the system.

The following points should be considered:

  • The SpaceLogic C-Bus Commission software allows the dimmer channels to be configured to restore any fixed level, or restore to their previous level upon restoration of power.

    • By default, all channels are set to restore to their previous state, with the stored previous state being OFF.

  • On restoration of power, the dimmer waits approximately 5 seconds for power to stabilize before restoring the channel states.

  • If a dimmer channel loses power, upon recovery of power, the channel is held OFF for the Power On Delay time programmed for that channel (default set to 0).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?