Arranging the Window

You can rearrange the tabs within the Archive Explorer application in one of the following ways:

  • Open any tabs by selecting them from the Window menu.

  • Select the tab that you want to move, and then select New Vertical Tab Group or New Horizontal Tab Group from the Window menu. This positions the tab in a separate area of the window.

  • Click and drag the tab to different areas of the window. A gray box appears when the cursor touches a border to indicate where the tab can dock.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?