Order

The Order Details tab displays data about the switching order. You can click the Name or Remarks fields and edit them. You can also select a value from the drop-down menu in the Region field. All other fields are read-only. The Approved and Planned fields are populated with a date and time stamp indicating when the switching order was approved or scheduled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?