Edit Hazards

Archive Explorer offers two ways to access and edit information about hazards associated with an incident.

  • From the Edit Incident window, right-click a hazard on the Hazards tab and select Edit. The Hazards tab displays all hazards associated with the incident.

  • On the Archive Explorer Incident tab, expand the incident to display the hazards associated with it, right-click a hazard, and then select Edit.

You can edit most of the hazard information. You cannot edit fields in gray. The Highlight, Zoom To, and Pan To tools are enabled only if you have ArcMap open.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?