Edit Call

From the Edit Incident window, right-click a call on the Calls tab and select Edit. This allows you to view the customer data as it appeared at the time of the call. Edit the fields as needed. Fields in gray cannot be edited.

You can delete a call, or multiple calls (with permission), by right-clicking the selected calls and selecting Delete.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?