Zoom to Incident Extent

Available in ArcMap. 

This tool modifies ArcMap's display to show the incident device and all features affected by it.

  1. In ArcMap, locate the incident device on the map.
  2. Click Zoom to Incident Extent  on the Responder toolbar.
  3. Click an incident device.
    A layer must be set as selectable before this tool can snap to its features. The map display zooms in or out to include all of the features affected by the incident device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?