Add Hazard to Incident

Available in Responder Explorer.

This tool allows you to indicate where a hazard exists and associate that location with an incident in the vicinity. An incident can have multiple hazards.

  1. Right-click an incident and select Add Hazard.
  2. Click the location where the hazard exists.

    In ArcMap, the cursor appears as a circle with a blue dot in the middle (the blue dot snaps to devices and lines alike). The cursor snaps to any feature (network and non-network) that has the RXHAZARD model name assigned.

  3. In the Edit New Hazard dialog, modify the Hazard Type and Wire Owner.

    The Edit New Hazard dialog displays information about the hazard. Only fields displayed in white can be edited.

  4. When public safety officers arrive at the scene, indicate their Time of Arrival and, after the hazard has been eliminated, their time of departure.
  5. Use the Remarks field to type any pertinent additional information.
  6. Click OK to add the hazard to the selected incident in Responder Explorer.
    NOTE: Multiple hazards can be added to a single incident.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?