Edit Location Feature

Archive Explorer offers two ways to access and edit information about location features associated with an incident.

  • From the Edit Incident window, right-click a feature on the Location Features tab and select Edit. The Location Features tab displays all non-electric features associated with the incident. Multiple rows can exist for a single feature. They display each operation on the feature (e.g., confirm, resolve).

  • On the Archive Explorer Incident tab, expand the incident to display the location features associated with it. Multiple rows can appear for a single feature. Each row represents an operation on that feature. Right-click the feature and select Edit.

You can edit feature information such as the region, time of report, and confirmed status. You cannot edit fields in gray. The Highlight, Zoom To, and Pan To tools are enabled only if you have ArcMap open.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?