Find Incidents

Available in Responder Explorer.

The Find and Find Next buttons allow you to search for specific incidents in the Incidents, Crew Assignments, and Incident Devices tables.

  1. Click the Find button and select the table and field that you want to search.
  2. Type a search value in the last field and click Find.
  3. Click the Find Next button to go to the next record that meets your search criteria (if applicable).

    If the search field has a data type of String (e.g., Remarks fields), the Exact Match field becomes enabled. Deselect this field to return all values similar to your search value (no wildcards are necessary).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?