Use as Incident Address

An incident uses the address of the first device, hazard, or location feature assigned to it. However, you can change the Address field to reflect the address associated with a device, location feature, or hazard assigned to the incident.

To change the Address field value on the incident, do the following:

  1. Right-click a device, location feature, or hazard on the incident, and then select Use As Incident Address.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?