Auto Change

Available in Responder Web Browser.

Auto Change allows you to automatically set modes at specific times, similar to setting an alarm clock. First, you set a time for a particular mode to become enabled. Next, you set Auto Change to Enabled. If Auto Change is disabled, the modes do not automatically change, even if they're set. Click List to view and edit existing mode changes or create new ones.

Primary Mode: The value displayed in the Mode field is the Primary Mode. This is the mode used if Auto Change is disabled. In the example shown in Insert New Auto Change Time, the primary mode is "night" and Auto Change is disabled. Therefore, "night" is the mode currently in use.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?