Switching Order Library

Available in Responder Explorer.

Unassigned switch orders and switch order templates are stored in the Switch Order Library. To open the Switch Order Library, select File > Switching Orders in Responder Explorer.

Click Open a Switching Order or Template from the Library or Create a Switching Order from a Template to view the library. Select Create a Switching Order or Create a Template to select a location in the library to store your switching order or template.

You can also access the Switch Order Library through the Switching Order Editor. Once you have the Switching Order Editor open, select Order > Open or Order > New.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?