Create Snippet Category

When you create a new snippet in the Create Snippet dialog box, you can also create a new category. To create a new category, type a new category name in the Category field. When the new snippet is saved, the category is also saved. If you don’t want to create a new category, you can instead select an existing category in the Category drop-down list.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?