Toolbar

The Responder Map Viewer toolbar is available at the top of the map.

Tool

Description

 Previous Extent

Moves the map display back to the previous display.

 Next Extent

Moves the map display forward to the next display. This button is enabled after you've clicked the Back Extent button.

 Zoom Out

Displays a smaller extent with the current map view as the center.

 Zoom In

Displays a larger extent with the current map view as the center.

 Full Extent

Zooms the map display to include all features in the map.

 Pan

Click this button to Pan the map display. This tool is enabled by default.

 Zoom Out with Rectangle

Draw a rectangle to zoom the map display out. The area indicated with the rectangle becomes the center of the map.

 Zoom In with Rectangle

Draw a rectangle to zoom the map display in. The area indicated with the rectangle becomes the center of the map.

 View Map Inset

Use this button to indicate a portion on the map to be displayed in the Map Inset window (see Toggle Map Inset below). Select the View Map Inset button and draw a rectangle on the map. Responder Map Viewer then exposes the Map Inset window with the display set to the area you highlighted with the View Map Inset button.

XY Coordinates

This portion of the toolbar displays the XY coordinates for the cursor's current location on the map. If the cursor is not in the map, this field is empty.

 Toggle Layers

This toggle button displays or hides the available map services and the layers within those services. Select the checkbox next to a map service or an individual layer in order to display it on the map. Clear a checkbox to hide the corresponding map service or individual layer. Map layers appear in gray when the map is zoomed out too far to see them.

 Toggle Overview Map

This toggle button displays or hides the Overview Map which shows the user's position on the main map relative to a smaller-scale inset map.

The Overview window in the top right corner shows the zoomed area in a map with a smaller extent. The current display area is highlighted by a blue shaded box with a red outline in the Overview window.

 Toggle Map Inset

Click this button to display the Map Inset Viewer window and its tools. This window allows you to zoom into a portion of the map without changing the main display. A corresponding red box in the main display illustrates the area of the map you're zoomed into. Use the Pan, Zoom, and Identify tools in the Map Inset window to navigate the map in the window or identify features. You can also use the View Map Inset tool to select an area on the map to be displayed in the Map Inset window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?