Snippets

Available in Responder Explorer.

A snippet includes a set of operations. This is useful if there are a particular set of operations that are frequently used. Rather than repeatedly creating the operations, with the proper roles and permissions, you can select a snippet and easily add the frequently used operations to the switching order with a double-click.

The Snippets tab allows you to save, access, and delete snippets.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?