Additional Tools

When you hover the cursor over the numbered circle associated with a row in the Attribute Viewer, you can access three tools that allow you to navigate to that particular feature.

  • Zoom To Feature: Zooms the map display to that feature.

  • Pan To Feature: Pans the map display to that feature.

  • Remove Feature From Results: Removes that feature from the selected set. This removes it from the Attribute Viewer and removes the corresponding marker on the map as well.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?