Disable Pop-up Alert Window: 

Accessible from the main menu (Window > Disable Pop-up Alert Window), this option allows you to disable all pop-up windows associated with alerts. A green check mark next to the option (as shown in the image below) indicates that alert windows are disabled. Alert windows are enabled when the green check mark is absent. Click Disable Pop-up Alert Window to enable or disable pop-up alert windows as needed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?