One Device Part of Multiple Incidents

Responder allows for a device to be added to more than one incident. The device must be in a Normal state on any and all incidents that it's a part of at the time of addition to a new incident. For example, if a device is part of a Switching Order (SO) Incident, and it has been opened and then closed back to a Normal state, a tool such as Create Fault or Add Fault could be used to add a fault on this device on an entirely different incident.

NOTE: Unexpected results occur when users encounter a scenario that includes the following three conditions:
  • Two SOs are open in the Switch Order Editor in two separate browser tabs.

  • Each SO contains a step that has the same device assigned.

  • Each SO is part of a different incident.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?