Assigned Switching/Restoration Order

Use these steps if the switching or restoration order has been assigned to an incident. A template is never assigned to an incident.

  1. In Responder Explorer, expand the incident that has been assigned to the switching or restoration order.
  2. Right-click the switching or restoration order and select Edit.
  3. Use the Switching Order Editor to edit as needed.
  4. When you've finished editing the operations, click Save from the Order menu and close the window.
    NOTE: If you click the red X in the window's upper-right corner, the entire window closes, along with any other switching orders in the window. If changes have been made to any switching order, a prompt appears for you to save the changes for each order.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?