Tabular

This tab displays data in a tabular format. Select the data that you want to view from the drop-down menu.

  • Customer Status: This data displays the number of customers in each region and the number impacted by an outage.

  • Interruption Status: This data displays the number of interruptions in each region and data about the number of interruptions with crews assigned.

  • Crew Status: This data displays the total number of crews and the percentage assigned to incidents and hazards.

  • Hazards Status: This data displays the number of hazards and the percentage assigned to crews.

  • Calls Status: Displays the number of active calls in the system and the number of unassigned calls.

  • Region Estimated Time of Restoration: Shows the estimated time of restoration for the selected region. If you have selected a region that contains other regions, the estimated times of restoration are displayed for each sub-region. This value reflects the estimated time of restoration set on the Restoration Estimates page in the Dispatchers section.

  • Feeder Estimated Time of Restoration: Shows the estimated times of restoration for the feeders in the selected region. These values reflect the estimated times of restoration set on the Restoration Estimates page.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?