Edit Auto Change Time

  1. Next to the Is Auto Change Enabled? field, click List .
    This expands the fields necessary to edit an existing Auto Change time.
  2. Next to the Auto Change time to edit, click Select.

    This populates the Mode and Start Time fields for the Auto Change time. The selected row is highlighted

  3. Edit the Mode and Start Time fields as needed.
  4. Click Update to save changes.
    The Status field displays the status of the operation (i.e., Update).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?