Close Incident

Available in Responder Explorer.

After the incident device has been completed, it must be closed as well. If the incident has outstanding callbacks, it cannot be closed until they are completed. Once an incident is closed, it is removed from Responder Explorer.

  1. Right-click an incident and select Close.
    If all callbacks have been completed, the incident is closed automatically. If callbacks still exist, the incident cannot be closed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?