ArcFM Overview

ArcFM consists of a family of geodatabases, which are intelligent sets of objects that represent the behavior and characteristics of landbase and utility features, plus an application layer that is an extension to ArcGIS. ArcFM allows utility businesses to make use of a single integrated environment to manage and map multiple utilities.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?