Default User Names

The Session Manager database offers default user names for each role in the sample process flow. SessionManager.mdb does not require a password when logging in.

Role

User Name

Session Administrator

Adams

Session Approval Officer

Applebee

Session Editor

Eddington

TIP: The names in the table above are sample names from the Schneider Electric same data.

Permanent user names must be set by your administrator in the Process Framework Administration Tool.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?