Classic Network Adapter Overview

Classic Network Adapter provides users with an interface to export a selected feeder from the geodatabase and import it into Windmil, a third-party analysis tool.

Use the Multispeak toolbar in ArcFM to import from and export to Multispeak.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?