Create Duct Connections
The Create Duct Connections task allows you to add connectors and splices to depict the travel of conduit through underground facilities such as vaults and manholes. This section describes how to use the Create Splices tool to add splices and the Create Duct Connections tool to add connectors to an underground facility.
- Select the Create Duct Connections task.
- Create connectors with Generate Duct Connector by first selecting the connector subytpe you want to add to the map from the Create Duct Connectors drop-down menu.
- Click Generate Duct Connector
and select
the first duct and then the second duct. The connector is automatically
drawn between the two selected ducts. - If you want to place a splice on the diagram and add connectors to it using Generate Duct Connector, first use the Create Splices drop-down menu to select the splice subtype.
- Click Place Splices
and add the splice to the map using the splice cursor
. - Click Generate Duct Connector
and click
a duct and then click the splice (or vice-versa). A connector line
is automatically drawn between the duct and the splice. Continue drawing
connectors to the splice in the same manner. The connection between
ducts and splices are automatically drawn on the map as shown in the
following example.
- Create connectors with Sketch Duct Connector by first selecting the connector subtype you want to add to the map from the drop-down menu.
- Click Sketch Duct Connector
and
select a duct to start the sketch. Draw a sketch with as many vertices
as needed. Complete the sketch by clicking on the second duct. - If you want to place a splice on the diagram and add connectors to it using Sketch Duct Connector, first use the drop-down menu to select the splice subtype.
- Click Place Splices
and add the splice to the map using the splice cursor
. - Click Sketch Duct Connector
and click
a duct or splice to start the sketch. Draw the connector with as many
vertices as needed and click the subsequent duct or splice to finish
the sketch. The following example depicts connectors drawn on a map
using Sketch Duct Connector.