Conduit Manager Overview

ArcFM Conduit Manager is an integrated set of tools and dialogs to add, annotate, and maintain the underground infrastructure of the utility network system. This powerful set of tools provides the ability to create and manage conduit, underground structures, duct banks and associated annotation. View the details of your underground structures such as duct bank placement and duct configuration. Tools such as lasso and cross-section annotation make labeling diagrams and features easy.

Conduit Manager tracing functionality is available without a Conduit Manager license. It allows you to trace the underground network and identify available ducts. All other Conduit Manager tools are disabled unless you have the correct licensing.

Conduit Manager requires proper licensing. Contact Schneider Electric for more information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?