Conductor Properties
Use Conductor properties to modify the conductor impedances used in the Voltage Drop and Fault Calculation.
Secondary Circuit Analysis uses conductor impedances from MMENG_CONDUCTOR_ELEC, looked up in the following order:
-
Size, Material and Insulation Type
-
Size and Material
-
DEFAULT
-
First row
If a conductor’s size, material and insulation type has a match in MMENG_CONDUCTOR_ELEC, then Secondary Circuit Analysis tool uses the match.
If it fails to find a match, the tool looks for a match on just size and material and if a match exists, it uses that.
If it still fails to find a match, the tool looks for an MMENG_CONDUCTOR_ELEC entry with a type of DEFAULT, and if a match exists, it uses that.
If that also fails, it uses the first row of the MMENG_CONDUCTOR_ELEC table.
To access the Conductor Properties menu, right-click a conductor in the Secondary Circuit Analysis window and select Properties from the resulting menu.
Here you can modify the conductor type and length to automatically recompute the impedance values. Uncheck the AutoCompute Impedances checkbox to modify resistance values for impedance.