Open Session Manager
Available in: ArcFM (Session Manager toolbar), ArcFM Viewer for ArcGIS Engine (Session Manager toolbar)
Enable: No session currently open
Session Manager may be opened from ArcMap by
clicking the Open Session Manager
button on the Session Manager toolbar. It may also be accessed as
a standalone application in the Bin folder of the ArcFM directory.
For example, D:\Program Files (x86)\Miner and Miner\ArcFM Solution\Bin\ProcessManager.exe.
If you open Session Manager as a standalone application, the Open
Session button will not be visible.
- Open Session Manager by clicking the Open Session Manager button on the Session Manager toolbar in ArcMap or access it as a standalone application.
- If you have Workflow Manager installed, you may select which extension you'd like to access: Session Manager, Workflow Manager, or both. If you have only Session Manager installed, skip to step 3.
- Enter your login information in the Login screen and click
Login. If you are logging into an Oracle or SQL database, a user name
and password are required. If you are connecting to an Access database,
only a user name is required. If you are logging into a secure Access
database, enter the correct user name and password for the database
on the Process Framework login screen. IMPORTANT: If you are using a secure Access database, the *.mdw file must have the same name as the Process Framework database and must be stored in the same directory.
If this is your first time logging in or your database connections have changed, you may need to edit the Database Connection Properties. You may also use default user names provided with the installation.