Disassociate Underground Conductor

To disassociate a conductor from a conduit system feature, you must select the conductor feature. Disassociating a conductor from a conduit entirely removes the relationship between the two features.

Right-click the conductor and select Disassociate from Conduit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?