Send to Design

A compatible unit (CU) can be sent to the Design tab on the Attribute Editor from a few different places. How Designer assigns the work function depends on how the CU is sent to the Design.

  • Selection tab: Right-click and select Send to Design. You may use the Work Function Tool to modify the work function.

  • CUs tab: Select a work function in the Work Function field at the top of the tab, right-click the feature and select Send to Design.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?