Zoom To

To change the map display to include selected features, use the Zoom To utility.
  1. Right-click a feature or layer on the Selection tab of the Attribute Editor or in the results tree of the Locator tool.
  2. Select Zoom To and the map view changes so that the features or layer are visible. Use the Highlight utility to see the features or layer flash three times on the map.
    TIP: Zoom To appears in blue text in most context menus because it is the default tool. If you double-click a feature, the default action (Zoom To) is performed.
    NOTE: You can change the extent to which this tool zooms. Click Customize > ArcFM Options > General tab, and change the Zoom To Buffer Size or its units.

     

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?