Conduit Manager Contents Trace

The Conduit Manager Contents Trace tool allows you to identify conduit contents between two trace points. This trace works in both Feeder Manager 1 and Feeder Manager 2. To run a Contents Trace, follow the steps outlined below.
  1. Click the Conduit Manager Contents Trace tool on the ArcFM Solution – Conduit Manager Trace toolbar.

  2. Click once to place a flag at the starting point of the trace, then click a second time for the trace end point.
  3. Trace results are displayed on the Conduit Contents Trace Results dialog. The trace results include conduit paths, listed by Feeder ID, with continuous feeders between the two trace points indicated in the previous step. The list also indicates the number of structures each individual conduit path passes through.
    You can also narrow your results by using the Search box. Type a Feeder ID in the Search box to filter the displayed results.
  4. Select a conduit path from the Conduit Trace Results list and the path highlights in the Map View.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?