View Field Information and Domain Information

We have brought back functionality in 10.2.1d that was removed in an earlier version. This right-click menu provides a way for users to view additional information about a field or domain without having to start an edit session.

Field Information

To access Field Information, right-click a field at the feature level in the Attribute Editor, then select “Field Information.”

The Field Information window then opens listing the field information for the selected field.

Domain Information

To access Domain Information, right-click a field at the feature level in the Attribute Editor, then select “Domain Information.”

The Domain Information window will open listing the available coded values for the domain associated to the selected field.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?